Part Number: PMP23391
Tool/software:
Hi,
Could you share the datasheet of CP-D1549-BZ?
I tried to contact the vendor but there is no response.
If it's not available, please share important specifications.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP23391
Tool/software:
Hi,
Could you share the datasheet of CP-D1549-BZ?
I tried to contact the vendor but there is no response.
If it's not available, please share important specifications.
Thanks.
Hi David,
I am not able to share the document. The key design specs are:
Pri : Sec = 5 : 4
L_pri = 22 uH, use shim inductance + leakage to control ZVS conditions.
Is their power spec the same as PMP23391? Below are the current stress calculations:
| Component | Peak Current | RMS Current |
| Primary winding | 22.4 A | 16.5 A |
| Secondary winding | 27.5 A | 15.1 A |
| Output inductor | 27.5 A | 22.0 A |