Part Number: TIDA-00121
Tool/software:
I have referred TIDA 0121 , I would like to configure the Dusk-to-Dawn Operation such that the system automatically switches the load on at dusk and off at dawn, based on ambient light levels, to ensure optimal energy efficiency. The proposed operational sequence is as follows:
- First 4 Hours: Full brightness (100%) .
- Mid 4 Hours: Reduced brightness (50%) .
- Last 4 Hours: Full brightness (100%) .
Kindly advise on how to proceed with this configuration. Please help