This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5013: TI Webench issues for the LM5013

Part Number: LM5013
Other Parts Discussed in Thread: LM70660, LM70860

Tool/software:

Hello experts, 

I've been trying to use the TI 'WEBENCH' Power design tool to get design suggestions for the LM5013 device.

Unfortunately, although I'm placing parameters within the accepted specs, I get error notifications saying the "Design cannot be created" with my inputs.

The specs are - INPUT: 35V-75V OUTPUT: 24V at 3.5A

Please see below and support. Thanks!