This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28911: UCC28911: UCC28911D - Usage for wide range input flyback

Part Number: UCC28911
Other Parts Discussed in Thread: UCC28881

Tool/software:

Hi,

Can you suggest IC with internal MOSFET for application.

Input voltage range 19V to 60V DC and 20V to 265V AC.

Output of 12V, 80mA.

Flyback. Duty requirement might be up to 90%.

We have size constraints and need cost optimization. 

Regards,

Anurag