Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA amplitude-modulated input source, how ?

Hello,

Is there a way to have an amplitude-modulated input source to my circuit ?

I need a 5MHz carrier signal, modulated by a 200KHz signal.

Is this possible ?

also, is it possible to add white noise ?

Thank you ..

  • OK, I figured it out ...

    It turns out that it is not easily done in the basic-free version on Tina because the "user defined function" is disabled.

    I tried a trial full version and was able to generate a modulated signal using the equation editor in the function generator:

    { Use this template to create your
      own signals }
    Function Signal(t);
    Begin


    A:=0.1;
    m:=1;
    fm:=200000;
    fc:=5000000;
       Signal := A*((1+m*cos(2*pi*fm*t))*cos(2*pi*fc*t));

    End;

  • rfengr,

    Alternatively, you can simply use two voltage sources and multiply them together (using POLY(2) VCVS for instance)

    Herman

  • Thanks Herman,

    I haven't tried your way, but I really like the equation editor method. I was able to generate a ringing effect using the equation below.

    By the way, what language does this equation editor use, are there any references out there on how to setup variables, functions, etc .. ?

    { Use this template to create your
      own signals }
    Function Signal(t);
    Begin
    A:=0.0005;
    m:=1;
    fm:=200000;
    fc:=5500000;
       k    := 0.0000005;
       mysig1:= 2/2.71828183^(t/k);
       Signal := mysig1*A*((1+m*cos(2*pi*fm*t))*cos(2*pi*fc*t));

    End;




  • I do not know the answer to your question, but I can ask around. Which full version do you use? 7.x or 8.x or 9.x?

  • Dear Herman,

    Can you please explain further how this can be done?

    Perhaps you can show the diagram.

    Thanks

    Mat