This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010054: SFRA Start Button from main.syscfg causes cryptic error message

Part Number: TIDA-010054
Other Parts Discussed in Thread: SFRA

Tool/software:

Hello,

I am working on TIDA-010054 Refboard with CCS V20.2.0.12_1.8.0, using  GUI  'main.syscfg'  to configure the lab and specific tresholds and so on;

In general the configuration works as intended, I am able to generate code and run the labs on the board;

It stucks within lab2, when attempting to press the 'RUN SFRA'  button; the SFRA tool does not start, instead there comes up an error message....

   

I have no idea to fix it, maybe someone can give me a hint.....

Friendly regards 

Martin