Part Number: LM5148
Tool/software:
Hi Team,
The LM5148 and ext. MOS will become hot around 45 degreeC wihle no load is attached.
After checked, when Vin=25V, the 12V output of LM5148 will be hot.
And the current is about 55 mA, as read from the power supply.
Is that normal or not?
If not, what can I check for this issue?
Thanks.