Part Number: TPS63000
Tool/software:
I have a design utilizing TPS63000 to generate an adjustable voltage output between 1.2 and 5.5V.
To allow for the voltage output adjustability the lower resistor of the voltage divider feeding the FB pin is tied to a current sink. The resistor between output and feedback is 16.2k due to the current sink.
This has worked well for a number of years, however, recent batches of boards are showing instability, the output of the regulator periodically oscillates.
As a first step, I would like to verify the phase margin of the nominal design but I am unable to generate a bode plot with Webench, am I just not seeing this option or is it not available for the TPS63000?
On a side note, the use of the current sink may reduce the gain margin the the regulator feedback loop, any suggestions on compensation?
Nominal inductor value is 3.3uH, reducing it to 2.2uH helps with stability.
Likewise, output is a pair of 22uF caps, increasing their rated voltage (and thus increasing derated value) as well as increasing nominal value helps with stability.
Thanks.