Part Number: TIDA-01238
Tool/software:
Hello,
To engage the termination resistor on FET solution, only U4 should be turned on by driving its gate to 5 V. Therefore, JMP9 should be connected to VCC and JMP10 to GND (to keep U3 turn off), correct? The purpose of U3 (CSD17483F4T) is to act as a voltage level shifter when using a 3.3 V microcontroller to control U4, and also to provide protection to the microcontroller I/O pin in case of high voltage on the CAN bus, correct?