This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02013: Why Is Isolation Used for the Low-Side GaN FET in a Half-Bridge with LMG3522R030?

Part Number: TIDM-02013
Other Parts Discussed in Thread: LMG3522R030, , ISO7710

Tool/software:

Hi,

I’m going to make an EV charger using TI’s GaN FET solution LMG3522R030, and I’m using the evaluation board TIDM-02013 as a reference. I have a question: why is the ISO7710 isolator and an isolated push-pull power supply used for the low-side GaN FET in a half-bridge? On the board, PGND is made common between the power side and the control side. I understand the need for isolation on the high side, but I don’t see the reason for it on the low side.

Thanks,