WEBENCH-POWER-DESIGNER: ESR for polarized capacitor in Webench Designer

Part Number: WEBENCH-POWER-DESIGNER

Tool/software:

Hello, 

I would like to create a custom polarized capacitor, but I'm not sure what to specify for the ESR as the value depends on frequency. Could you clarify on this matter? 

Thanks

  • Hi Khoi,

    Following are the two ways to determine the ESR of the polarized capacitor.

    1. If datasheet specifies a value at 1 MHz, use that value of ESR

    2. Else if datasheet shows a ESR (or impedance) versus frequency graph use the bottom-most value.

    Kindly revert back to us for any further queries.

    Thanks and Regards,

    Umayal