This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146-Q1: LM5146QRGYTQ1 - Schematic Verification

Part Number: LM5146-Q1

Tool/software:

    

Hello TI Team,

I’m requesting a quick design review for my LM5146-Q1 synchronous buck controller. The application is automotive. Details and files are below. Please let me know if you see any issues or have recommendations.

Thank you!

— Muthukrishnan
Embedded Engineer, Dotworld Technologies Pvt Ltd

  • Hello,

    I recommend filling out the quickstart calcualtor as well to check your design, particularly power losses and compensation.

    1. No need for diode D2.
    2. Add local cap at the VIN pin.
    3. The VCC cap should be 0603 or 0805 and placed close to the IC. No need for 100V rating (large cap).
    4. The NC pins can be grounded for better heat spreading.

    Regards,

    Tim