This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01344: Question on How to Alter for System Requirements

Part Number: TIDA-01344

Tool/software:

Hello TI,

We are looking to design a flyback controller similar to the TIDA-01344. But we need a wider Vin range of 15 to 140V to account for a 24-96V battery system. With 12V Vout and 2A nominal 3A peak output current.

Could we use still use the flyback transformer model UA8263-AL specified in the design? If so, how can we change the design to meet our requirements?

Thanks in advance,

Best Regards, Makersan R&D