This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP21274: Inductor select

Part Number: PMP21274
Other Parts Discussed in Thread: LM5122, , LMR36015

Tool/software:

Hi team,

My customer is evaluating with LM5122, and they are reference the PMP21274 design

However the inductor is too big, can you please help them simulate the minimum Isat/Irms_max that they needed?

Their Application:

Vin range: 12V~55V

Output: 55Vin

1. 120W output power(Iout 2.18A), minimum Isat/Irms_max 

2. 240W output power(Iout 4.36A), minimum Isat/Irms_max 

Thanks