Part Number: PMP41062
Tool/software:
Hi
On the PMP41062 webpage, PMP41062 reference design | TI.com, you kindly give the gerber files and the BOMs.
However Is it possible to have the "Pick and Place" / "Component Place List" file for the components?
I'm looking for this format in a spreadsheet if possible as an example.....
| Designator | Mid X | Mid Y | Layer | Rotation |
| C1 | 95.0518mm | 22.6822mm | Top | 270 |
| C2 | 106.4056mm | 23.0124mm | Top | 90 |
| C3 | 109.0726mm | 22.8854mm | Top | 270 |
| R2 | 109.5996mm | 16.6443mm | Bottom | 0 |
I hope that this is possible please.
Many Thanks
Richard