Part Number: PMP41115
Tool/software:
Hi,
I am looking to design a board similar to PMP41115 that will operate with 30 - 40V battery voltage instead of 42V and 50V as shown in the reference design. The 240W output should be able to be sustained without hitting thermal limits for about 22 minutes, within a plastic casing that may or may not include additional heatsinking measures other than those related to the PCB (via stitching, 4 layers, 2oz copper) based on feedback here.
With these parameters, I've assumed that the main power losses are within the inductor and MOSFETs, so I have chosen alternative components that could yield greater efficiency.
Inductor CMLB136T-100MS --> B82559A7103A020 (lower DC and AC losses)
MOSFET SIR880BDP-T1-RE3 --> ISC0602NLS (higher Rds(on) but lower gate charge)
Could you please give me a rough estimate of whether these changes might be sufficient for the device to operate within these thermal conditions? Are there any other large sources of losses that I could reduce with bigger or more expensive components?
Thank you.