This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP40988: Question consultation

Genius 14510 points

Part Number: PMP40988

Tool/software:

图腾柱pfc过零点畸变.pdf

Hello, I'd like to ask a few questions.

1. Single-phase totem pole PFC has zero-crossing distortion of inductance current, which can be eliminated by using soft start according to the document. If, according to PMP40988, after staggered parallel connection, the two-phase switch tube lags behind the main phase for half a period, then how to realize soft start to avoid zero-crossing distortion? How to open the tube of master phase and slave phase?

2. There is Ton in 2:PMP40988, which is the CrM/TCM PFC controlled by voltage COT. How to model the transfer function from output voltage to constant on time Ton, is there any reference?