This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161: The power output affects the accuracy of sensor

Part Number: LM5161
Other Parts Discussed in Thread: LM5160

The problem we are currently encountering is that when using the LM5160DNTJ chip and the isolated power supply application solution, the voltage variation after isolation has an impact on the accuracy of the subsequent sensor when the input voltage changes.

The following location issue has been identified. Disconnecting resistor R131 and supplying power to the subsequent stage from another source is fine. By adjusting R136 and C140, there has been an improvement, but the effect is not satisfactory. Could you give some advise,thanks.

The problem is located in the red boxTOPOLOGY.jpgsch.pngThe influence of power supply changes on accuracy.png