Part Number: AFE7950EVM
Other Parts Discussed in Thread: LMK04828, AFE7950
I have the version of latexx 2.9 and the AFE7950EVM board. When I try to run AFE.deviceBringup() i get some erros. See following image. Why is this hapenning?
Another question. I want to control the FPGA_REFCLK2* frequency in addition to the GTXCLK that is already being configured. How can I do this in Latte? The FPGA_REFCLK2 is the signal name output from LMK04828 which goes into the FMC connector.
Another question. There is a signal called SYNCBOUT** that is an output of the AFE7950. What are the conditions for this signal to activate? In my setup I am using only TX (DAC) for early testing, and the syncing process is not starting, which is related to this signal.
Please advise