This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568230: Enable Max Limit

Part Number: TPS568230

Hi Team,

From Datasheet it seems EN pins absolute max voltage is 4v.
What will happen if I design EN voltage as 5V.

Will it cause any issue or works without any issue.