Part Number: TPS2595
This is my first time using an eFuse, so I would like to ask a few questions.
I'm planning to prototype a board using the circuit shown below. I will attach the schematic, so please let me know if you see anything concerning.

— Preconditions —
The circuit configuration is: USB Type‑C connector <-> TPS259530DSGR <-> DC‑DC / battery circuit.
The reason for using an eFuse is for CE and other certification tests. If an abnormal condition occurs in the battery circuit and the current exceeds the specified value (1 A), I want the eFuse to shut off the abnormal current.
Here are the points I'm a bit concerned about:
- Should I add a component to cut the current between the USB Type‑C connector and the eFuse?
If the eFuse can fail in a short mode, I would like to know whether adding a current fuse or something similar is preferable.
- I think the ceramic capacitor at the IN pin of the eFuse can be set as Not Mounted, but is that acceptable?
- Since the FLT pin (pin 6) is an open‑drain output, I think it is fine to leave it unconnected if the CPU does not monitor faults. Is that correct?