This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG36XX-CALC: LMG3522R030RQSR EMI Simulation

Part Number: LMG36XX-CALC

Hello,

I am working on a conducted EMI simulation of a high-power GaN inverter, and I need a SPICE/LTspice model for the LMG3522R030RQSR power IC (650 V GaN integrated driver + FET) to include in the simulation.

My use case is conducted EMI and switching transient analysis, so it is important that the model accurately represents EMI-relevant switching behavior (dv/dt, output capacitance behavior, and driver effects), not just loss or average behavior.

Specifically, I am requesting:

  • A SPICE/LTspice simulation model or library for the LMG3522R030RQSR that can be used in LTspice, suitable for EMI and high-dv/dt transient simulation.

If a model for that exact part is not available, I would be grateful for:

  • A recommended 650 V GaN power IC (integrated driver + FET) with a publicly available LTspice model that includes EMI-relevant switching detail.

Please let me know if such a model can be provided. Thank you very much for your assistance.

NOTE: This part was not available on the drop-down menu, so this is likely categorized under the wrong part.