This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR471TPEVM: Using DLP EVM GUI software library/API in a standalone Python application

Part Number: DLPDLCR471TPEVM

Software: DLP EVM GUI
EVM: DLPDLCR471TPEVM

Hello,
I am a university student who's part of a student semiconductor fabrication organization. We're using the DLP LightCrafter Display 471TP EVM as a UV projector for a lithography stepper.

We want to integrate both the DLP projector controls and stepper motor controls into a single standalone Python application. Currently, we're able to write Python projector scripts in the EVM GUI advanced mode using the projector API. However, we currently do not know of a way to connect to the EVM outside of the provided GUI software.

Is there any way to use the GUI API in a standalone application, or connect and send instructions to the projector outside of low-level I2C/USB commands? We're hoping to be able to upload images, change RGB values, and control exposure time.

If you have any additional or clarifying questions, please let me know. 
Thank you very much for your time.