Part Number: TPS7H4011-SP
I am trying to simulate the inverting buck-boost configuration of the TPS7H4011-SP using the official PSpice model provided by Texas Instruments.
My goal is to generate a negative output voltage starting from a +5 V input (for example −3.3 V or −1.5 V).
I implemented the circuit following the inverting configuration shown in the TPS7H4011-SP datasheet, but the simulation does not work as expected.
Observed behavior in PSpice:
-
The SW node does not switch.
-
The output voltage stays around −200 mV instead of regulating to the target negative voltage.
-
The controller appears not to start switching at all.
What I already checked:
-
EN pin is enabled.
-
ILIM resistor is correctly defined.
-
Inductor and output capacitor values follow the datasheet recommendations.
-
Feedback divider is calculated for the desired negative output voltage.
However, the converter never starts switching in simulation.
My questions are:
-
Are there any special pin connections required in the inverting configuration when using the PSpice model (for example COMP, RSC, REFCAP, or FAULT)?
-
Is there a known limitation of the TPS7H4011-SP PSpice model when simulating the inverting topology?
-
Could someone provide a working example schematic for the inverting configuration using this device?
Any guidance or example project would be greatly appreciated.