This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC110: AMIC110 Sotware link incorrect

Part Number: AMIC110

I am currently working with the AMIC110 ICE evaluation board and have encountered an issue with the official software documentation.

The provided software link:
http://processors.wiki.ti.com/index.php/AMIC110SW

appears to be broken or misdirected and does not provide usable resources for development.

As a result, I am unclear on the correct starting point for software development on this platform. The available SDK structure is very large, and there is no clear documentation on how to begin a minimal custom project for basic bring-up (UART, GPIO, timers) without relying on large example projects.

Specifically, I am looking for:

  • The correct and current software documentation or resource link for AMIC110
  • Recommended workflow for creating a minimal custom project (bare-metal or low-level)
  • Guidance on initializing basic peripherals (UART, GPIO, timers) on this device
  • Clarification on whether StarterWare is still a valid approach for evaluation/prototyping

My goal is to build a simple proof-of-concept relevant to industrial control (basic I/O, timing, and communication), but I am currently blocked by the lack of clear entry-point documentation.

Any guidance or updated resources would be greatly appreciated