Part Number: LM5156-Q1
Other Parts Discussed in Thread: LM5156



Hello,
I have attached pictures of the flyback circuit application of LM5156 chip. As you can see in first picture is that we use this chip to provide drive signal controlling the mos in the Second picture generating the primary voltage the transformer. Afterthat, the third picture showed that the Secondary side will create the 12V voltage to supply LM5156.
Now, we have set the switching Freq 219k Hz and slope compensation without Q241 part. The problem is about COMP pin. We find that the RC value is not good enough to control the output signal smoothly. We want a proper value of R and C to generate the 12V output with low ripple
The green line is the output of 12V. It has 0.3V ripple voltage. Blue line is the AUX-BUS input. Purple line is the waveform of COMP pin. We want smaller ripple voltage of 12V output.



And in what situation, the gate pin will generate this waveform.