Part Number: MSPM0G3519
Other Parts Discussed in Thread: LP-MSPM0G3507, MSPM0G3507
Greetings,

Given the above pinout, I need a sanity check and possibly warranty replacement ASAP!!! The Rx and Tx are:
I spent a few frustrating days trying to figure out why a ported application (from LP-MSPM0G3507 >> proprietary board with MSPM0G3519 ) wasn't communicating correctly. I can step through debugging and see that my FreeRTOS tasks are running- LEDs and buttons trigger- but the debugging messages weren't getting sent to the Application/User UART. After a few minutes, the XDS110 would disconnect altogether, but LED indicated application was still alive.
I just gave in and fired up the scope (the design was OK before, what could be wrong)?
I verified there is Tx data... Next, I plugged in the XDS110 AUX cable and the signal became corrupted. The MCU couldn't pull the below 3V and not able to drive a true low. I Disconnected the Aux cable connection and the RS232 Tx signal swing returned to 0V>3.3VDC.
This is the first we've used TI and this debug probe. Up until now we were developing on the LP-MSPM0G3507 with almost exact I/O circuits without issue.
Is there additional circuitry needed to use the back channel UART? Configuration in the ccxml?
Please expedite this, as we've lost a lot of time in porting our design.