This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Help using System Analyzer (UIA Target) for Execution and Load Analysis

Part Number: TMS320C6748

I am using SYS/BIOS 6.50.0.10, System Analyzer (UIA Target) 2.3.1.02, and XDCtools 3.50.2.20, for a TMS320C6748 Target. Our company has migrated everything to Windows 11, I had to transition from CCS 6.1.1 to CCS 7.2.0  for development. We are connecting with the Blackhawk USB560V2 System Trace probe

I have been trying to use the RTOS Analyzer to profile our target application (starting with execution analysis and Task/CPU load analysis). I started with the stairstep_JTAGstop example that comes loaded in the TI Resource Explorer Classic and am able to load/run the application on my target. The problem is the System Analyzer results are not what I am expecting. The CPU Load graph and Task Load graphs never render. The load values in the Detailed view of the CPU Load/Task Load graphs do not match the expected load values in the example.

As an initial sanity check, am I running a compatible environment? Should the SYS/BIOS, System Analyzer, and XDCtools versions I am using work for CCS 7.2 and Windows 11? Is there updated documentation for these versions of System Analyzer?