This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28710: UCC28710 Startup Issue

Part Number: UCC28710

Hello Team,
I have designed an AC/DC charger with specifications of 58V / 200W. 

During light-load test, output reaches 58V (design target). But when load current is gradually increased, converter shuts down automatically. After shutdown, converter does not restart.

Checked primary side:

  • Proper voltage present at HV pin
  • VDD capacitor charges up to 21V and then discharges repeatedly
  • No DRV pulse observed
  • No VS/CS pin activity

Please suggest the possible reason and solution for this issue.

Regards,

Kalyani