Part Number: TMDSEMU200-U
CUSTOMER ISSUE :
P/n: TMDSEMU200-U
"When we connected the Debugger first time to the Host PC, the power LED
on the debugger does not turn on and the device is also not detected in
the PC Device Manager under USB devices."
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSEMU200-U
CUSTOMER ISSUE :
P/n: TMDSEMU200-U
"When we connected the Debugger first time to the Host PC, the power LED
on the debugger does not turn on and the device is also not detected in
the PC Device Manager under USB devices."
Hello Venu,
Thank you for reporting this issue with your TMDSEMU200-U debugger. When the power LED does not turn on and the device is not detected in Device Manager, this typically indicates a power delivery or connection issue. Please work through the following troubleshooting steps:
USB Connection and Cable:
Power Supply:
Driver Installation:
Device Manager Verification:
Hardware Inspection:
Isolation Testing:
Please attempt these troubleshooting steps and report back with your findings. Specifically, let me know:
If the debugger still does not power on or get detected after these steps, we may need to evaluate a hardware failure and discuss replacement options.
Best Regards,
Zackary Fleenor
Please refer to the below customer response:
I followed all the suggested troubleshooting steps, but the TMDSEMU200-U debugger is still not working.
Based on these checks, it appears the debugger is not receiving power at all, and the issue is likely hardware-related.
Please advise on the next steps for hardware evaluation or replacement.
Regards,
Venu CK.
Hello Venu,
Thank you for thoroughly working through all of the troubleshooting steps and providing detailed results. Based on your findings, I agree that this appears to be a hardware failure with the TMDSEMU200-U unit. The fact that the power LED does not illuminate under any condition, across multiple cables, multiple USB ports, and multiple host PCs, with no device entry appearing in Device Manager at all, confirms that the unit is not receiving or responding to power, which points to an internal hardware defect.
To proceed with a hardware evaluation and potential replacement, please follow the steps below:
Confirm your purchase details including the date of purchase, the distributor or vendor you purchased from, and your proof of purchase or order number.
Visit the TI Support portal and submit an official hardware return or replacement request. You can reach TI's support team directly at https://support.ti.com to open a formal case for a defective unit evaluation.
If the unit is within the warranty period, TI will evaluate the device and determine eligibility for a replacement. If purchased through a distributor such as Digi-Key, Mouser, or Arrow, you may also contact them directly to initiate a return or exchange under their respective return policies.
Please provide your purchase details here as well so I can assist in escalating this further on my end if needed. I want to ensure this gets resolved for you as quickly as possible.
Best Regards,
Zackary Fleenor