Part Number: LM5155-Q1
Other Parts Discussed in Thread: LM5155
Hi expert,
Could you pls help share what happen if the LM5155 FB open at Sepic circuit? and pls provide the Pin FMEA doc, thanks.
BR,
Hangjie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hangie,
When FB is floating, its difficult to say what will happen. The worst case will be that there is 0V at FB and the duty cycle will increase to the maximum.
Then the output voltage will run away. I have to check if we can provide a pin FMEA.
Best regards
Moritz
Hi Moritz,
thanks for that, pls help share the Pin FMEA doc once you get.
BR,
Hangjie
Hi Hangie,
Sure, i will share it as soon as possible.
Best regards
Moritz