TPSM861253EVM: un-encrypted spice file for TPSM861253RDXR

Part Number: TPSM861253EVM
Other Parts Discussed in Thread: LM5118, TPSM861253

Hello, to whom this reach.

   I'm here on a request, for some time now i have been study the LM5118 data sheet and now finally generated a working schematic from a new project on PSpice for TI. On almost completion i received an email from a News Letter from Murata stating they have a new sensor which detects vibration for faulty ball bearing or electrical motor. For me to intergrage this to the newly generated schametic i need to lower my 12 Vout to 3v - 5v, this is how i came across the TPSM861253RDXR ic.

 

On me using the un-encrypted version of the LM5118 with no alteration, i will love to do the same with the TPSM861253RDXR.

 

Opening up the TPSM861253 PSpice file i notice the spice file where encrypted.

 

If possible, is there anyway i can get the un-encrypted spice file for the TPSM861253RDXR  ic?

 

thanks so much,

joel.