Part Number: LM5156-Q1
Other Parts Discussed in Thread: LM5156
I had utilized the flyback simulation of LM5156 provided by the TI itself. I had done some modifications in that for getting 28V as output since the TI provided simulation is for output 5V. I had modified flyback transformer ratio in the script itself. Ihad tuned feedback resistor in opto based feedback section.
Flyback ratio (Pri : Aux : Sec) : 1:1:3
Flyback transformer inductance : 15uH
Feedback bottom resistor value : 1.36k
But my output stayed at 5V only not increased to 28V. I'm using Orcad pspice 17.4 for my simulation