Part Number: AM263PX-RESTRICTED-SECURITY
Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
In the SysConfig of the HSM firmware for the MPU, L2OCRAM_BANK0_SLV, the initiators allowed to access the region 0x70000000 to 0x70080000 are R5FSS0_0, R5FSS0_1, R5FSS1_0, R5FSS1_1, and M4_0. The MPPA permissions are configured as User Read, User Write, User Execute, Supervisor Read, Supervisor Execute, with Non-Secure (NS) = 1 and EMU = 0.
With these settings, I am not facing any issues. However, if I change the NS setting in the MPPA configuration from 1 to 0, the SBL fails, and the error interrupt is triggered.
Can you tell me why this violation occurs when NS = 0? and also what is the difference between these non secure and secure access ?? How it will decide secure access is taking place?