Part Number: LM5066H1EVM
Dear sir,
This is regarding the GUI for LM5066Hx Evaluation module.
We are using LM5066H1 for our project, procured the EVM board and USB TO GPIO2 adaptor for demo. Now we need to download the GUI software to work in offline (without internet) mode.
The LAUNCH option of the GUI under 'order and start development' tab of LM5066HXEVM gives two modes: ONLINE and OFFLINE. But it was mentioned that OFFLINE here means virtual device. The site then prompted us to download a TI CLOUD AGENT. I downloaded, installed the cloud agent software to our work system without internet. The following list of folders and files are in the installed folder: drivers, resources, src, util, ccs, config, node, ticloudagent (windows batch file)).
When we click the link for the user manual for the GUI in the site, no pdf fil is getting downloaded. It is showing ERROR 404.
Pls share the user guide to install in offline mode or share the procedure to install.