LM5145-Q1: LM5145-Q1 Pspice Model issue

Part Number: LM5145-Q1

Dear Support Team, 

During simulation, we observed an issue related to the VCC external bias functionality. In our design, VOUT (12 V) is connected to the VCC pin through a diode, and this functionality works correctly during real-time testing on the evaluation board. However, in the PSpice simulation environment, the VCC pin does not switch to the 12V output voltage as expected.

I am attaching the PSpice model which we are using. Could you please verify whether this functionality is supported in the current PSpice model? Additionally, do you have any updated/latest PSpice model for the LM5145-Q1 that includes or better supports the external bias functionality for verification?snvmb65c.zip 

We appreciate your support and look forward to your feedback.