Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: UNIFLASH
Dear TI Support Team,
Good Evening,
My name is Mr. Amol Chavan from Kyoritsu Electric India Pvt. Ltd., Pune, Maharashtra, India - 411057.
Our target device is the TMS570LS043x microcontroller. We are using the XDS110 Debug Probes to program the target devices individually as well as in parallel.
We are using CLI (Command Line Interface) commands through the Windows Command Prompt for the programming process.
When we program the target devices individually, one at a time, the programming process completes successfully without any issues.
However, when we perform parallel programming using multiple XDS110 Debug Probes simultaneously, we are experiencing intermittent programming failures. For example, when we attempt to program 6 target devices simultaneously, approximately 3 to 4 devices generate errors, and the programming process for those devices fails. The remaining devices may complete the programming successfully.
We would like to understand the possible cause of this issue and whether there are any specific configurations or limitations related to parallel programming using multiple XDS110 Debug Probes with TMS570LS043x target devices through CLI commands.
Could you please provide your technical guidance on the following points:
-
Is parallel programming of multiple TMS570LS043x target devices using multiple XDS110 Debug Probes supported?
-
Are there any limitations when operating multiple XDS110 Debug Probes simultaneously on the same PC?
-
Is any specific configuration required to uniquely identify and assign each XDS110 Debug Probe to its corresponding target device when using CLI commands?
-
Are there any recommended USB configurations, such as using separate USB ports or USB hubs, when connecting multiple XDS110 Debug Probes?
-
Are there any recommended JTAG configuration or signal integrity considerations when programming multiple devices simultaneously?
-
Is there any specific CLI command-line option or configuration required for reliable parallel programming?
-
Could the issue be related to simultaneous access or resource conflicts between multiple XDS110 Debug Probes running in parallel?
We can provide the exact CLI commands, programming scripts, error logs, and error messages generated during the failed programming attempts if required.
CLI Command: "C:\ti\uniflash_9.6.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\DSLite.exe" flash -e -v -t 30 -c "D:\TMS570_PRODUCTION_PROGRAMMER\ccxml\TMS570_XDS00006.ccxml" -f "D:\TMS570_PRODUCTION_PROGRAMMER\firmware\18133586.hex" "D:\TMS570_PRODUCTION_PROGRAMMER\firmware\Manufacting Data Endurance 2 channel CCP 10-11-23.hex" > "D:\TMS570_PRODUCTION_PROGRAMMER\logs\Board6.log" 2>&1
We would appreciate your technical guidance in identifying and resolving this issue.
Thanks & Regards,
Mr. Amol Chavan
Mo. +91 9561337754
E-mail: amol@kyoritsuelectric.com
Board1.log Board2.log Board3.log Board4.log Board5.log Board6.log