Part Number: MSPM0-SDK
Other Parts Discussed in Thread: MSPM0G3105, UNIFLASH, LP-MSPM0G3507
I am using CCS 20.5 and the XDS110 USB Debug Probe.
The design uses a MSPM0G3105. The cpu is fresh from factory (it never been programmed with any code or configuration).
All the signals to the 10-pin debug connector are connected as indicated in the documentation:
Pin 1 = VTREF (connected to the board's 3.3V)
Pin 2 = SWDIO
Pin 4 = SWCLK
Pins 3, 5, 7, 9 = GND
Pin 10 = nRST
The .ccxml file is configured for SWD Mode and Target Supplied Power. I even reduced the frequency to 100 kHz.
In CCS, if I select Run/Debug Project, the session starts, but when it tries to load the program, it stalls at PT_LOAD[0]: 0 of 2344 at 0x0.
I tried "Start Project-less Debut", then Connect Target on the CORTEX_M0P thread. After that, I get the same result if I go through Run/Load Program.
I used the "Test Connections..." button in the advanced properties of the ccxml file and it says the SWD Mode Integrity test has succeeded.
I get the same results if I use UniFlash.
I verified my XDS110 USB probe is working properly with a LP-MSPM0G3507 Development Kit. It worked as expected and I was able to load and run a program in the CPU.
I need help with this issue (I tried multiple PCBs).