UCC28051: UCC28051

Part Number: UCC28051

I am doing some EVA calculation for the close loop system of UCC28051.
I can see that the gM E/A amplifier output is tied to COMP in the block diagram. 
The COMP pin has voltage ranges from 2.5 to 3.8V. But the gM E/A output is closely to  (2.5-Vo_sns)90uS.
1. This output is current in nature. How is this voltage converting into voltage ?
2. Is there any resistor diver circuit connected to the output of gM E/A ?
3. Can you please provide a schematic on how they are connected? and also provide the values if any?