Other Parts Discussed in Thread: TPS51315, TPS54620, LM20136, TPS54618, LM20146
For Vin=5V,Vout=1.05V/6A,looked at the TPS51315.
I used the SwitcherPro to generate a schematics, only thing I have changed was the output capacitor to a capacitor we do have in hand (T495D227K010R0100) which is a 220uF/ 10V/ 100mOhm.
I have noticed the report (Analysis - Output1 page) states 377mV as Output ripple p-p.
Is this is the expected output ripple? This is much above the allowed 50mV ripple for the CPU core ...
I have opened the TINA. The built in example in the TINA is also for 1.05V output with a load of 10Amp so I have used it and run it as is.
The ripple over Vout was few hundreds mV.
I have changed this circuit to match exactly the values presented by the SwitcherPro. The results were much worse than before (reducing the Cout ESR value from 100mOhm down to 10mOhm improved this situation but not better than the original result from TI own example.
It is hard for me to exit files, so I can not send you for now the TINA and the SwitcherPro files, but I will appreciate a lot if you can send me a design in SwitcherPro format, or better in the TINA format, that meets my requirements : best if 5V input and output of : 1.05V / 6Amp / 85c ambient / less than 50mV output