This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331 Power to high

Hello

I calculated a Design with SwitcherPro for

Vmin=15V

Vmax=26V

Vout=5V

Ioutmax=2,5A

Also I have a Design for 12V Output and one for 3,3V Output.

But my Output voltage is

5V instead of 3,3V

6,7V instead of 5V

16,7V instead of 12V

How can I reduce the voltage? I tried to change R2, but it doesn't work. Can I reduce the voltage, but keep the same Inductor?

5-12-3.3.PDF