I attempted to duplicate a design I've done previously on Webench .
When I enter the parameters and select a device, the system hangs with a blank screen and a URL (that it won't let me cut & paste into this message).
I'm using the following parameters: VinMin 22.0V
VinMax 26.0V
Vout 3.0V
Iout 0.4A
30 Deg C
Device LM2674-3.3
This design is the same as Design: 1125765/311 lM2674MX-3.3
I've attempted this 4 time now. What's up?
I'm running WIndows 7 Pro and Chrome on a Dell T1600 workstation. I've run this design and 310 others on Webench without problems.
Rick Barnich