Other Parts Discussed in Thread: TPS62110
I noticed that the values computed for the divider resistors for the FB pin (using a TPS62110) were in the 500K amnd 180 K range for 5V but for all other output voltages they were values like 510/180. I believe the Higher values are the correct ones. I sure the supply would work with the lower values though the resistors might get a little warm.
I also noticed that with an input voltage of 12V the program selected an capacitor C2 with a voltage rating of 6.3V.
SwitcherPro Desktop
Version 3.17.0.0
Built on 2011-10-28 02:37 PM
Copyright © 2012, Texas Instruments, Inc
Database Version 328
SystemParts Version 378