This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Import standart Spice model

Hi,

I'm trying to import a spice mode. (txt file) into Tina TI. The problem is that is always show this error : "Missing syntax element : Line#2". I don't know what's wrong... I'm trying to import Diode incorporated model, the component is BSS138W.

The spice model :

*SRC=BSS138W;DI_BSS138W;MOSFETs N;Enh;50.0V 0.200A 1.60ohms Diodes Inc. MOSFET
.MODEL BSS138W NMOS( LEVEL=1 VTO=1.20 KP=50.0m GAMMA=1.49
+ PHI=.75 LAMBDA=83.2u RD=0.224 RS=0.224
+ IS=100f PB=0.800 MJ=0.460 CBD=56.3p
+ CBS=67.5p CGSO=96.0n CGDO=80.0n CGBO=324n ) * -- Assumes default L=100U W=100U --

Can somebody help me please ?

Eric