Other Parts Discussed in Thread: LM5018, TINA-TI, LM5017
Pretty straight formward. Set up for 32-90Vin, 30V @ 0.25A output. Webench produced 3 solutions and I picked the LM5018. I used the default component calues but the sims do not produce output voltages as expected even though no errors are indicated. For example the load ransient does show a -/0.25A load but the output voltage is only at approx 7V (should be 30V). When I probe Vin it indicates a maximum of 75V and a nominal of 61, what gives with that? Similar funkiness with the startup and steady state.
Can this get resolved quickly? I need to proceed with this design and if I can't trust a sim with default components then I can't trust the result.