Hi,
Please help me get the eagle library for TPS55340.
Thanks a lot.
Q.Chu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q. Chu,
The TPS55340 was released 26OCT2012 and we do not have CAD symbols and footprints generated yet. I will submit a request to our vendor to produce both HTSSOP, PWP 14 pin and WQFN, RTE 16 pin. The turn around for the vendor is usually within 2 weeks.
Regards,
Janet
Q. Chu,
TI recently began providing Symbols and Footprints to customers in a new way. The Symbol and Footprint are together in a neutral format (in a .bxl file) which can then be translated to the desired Symbol and Footprint tool using a free translator called Ultra Librarian reader.
You can download bxl files plus the Ultra Librarian free reader by going to the WEBENCH page: http://webench.ti.com/cad/
The WEBENCH page points to Ultra Librarian download link:
http://webench.ti.com/cad/ULib.zip
Other bxls in the TI catalog can be found through a pattern search (no wildcards required) using the Search box.
Here is the link to the file listing all of the BXLs currently available on the website:
http://webench.ti.com/cad/pf_cad_data.txt
You can download Ultra Librarian getting started links from
http://www.accelerated-designs.com/Startup.aspx and
http://www.accelerated-designs.com/Demo.aspx
Regards,
Janet
Q. Chu,
The links for the TPS55340_PWP_14.bxl and TPS55340_RTE_16.bxl did not come through in the previous email so here they are:
These bxls will be published to web soon.
Regards,
Janet
Hi, i am trying to design high voltage dc dc converter by using tps55340, from 5v input to 900V output
isolated type, please tell me weather it is feasible with that ? the overall power would be around 3 to 4 W.
Y Nath