Hello,
For a moment I use "Custom LED" option to set parameters for CXA Cree LED.
Is it foreseen to add Cree CXA-series LED model to the WEBENCH® LED Designer?
best regards,
Oleksiy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
For a moment I use "Custom LED" option to set parameters for CXA Cree LED.
Is it foreseen to add Cree CXA-series LED model to the WEBENCH® LED Designer?
best regards,
Oleksiy
We're checking on this, but an answer may be delayed due to the holidays.
The parts had not been available at the distributors for a time. That should now be rectified. The database will be updated soon. Please check again in a couple of days. I tried setting up a design with 40V in, 900lm which looks to be in the range of the CXA-1507 (37V forward, up to 1400lm) but the tool didn't show that as a solution yet.
Best Regards,
David
David, thanks for the answer.
For a moment in the database only CXA2011 available. I'm waiting for updates.
best regards,
Oleksiy