Other Parts Discussed in Thread: LM5007, TINA-TI
Hi all,
I am trying to simulate the model of lm5007 in PSpice 16.5 demo/trial version. Please help me the procedure how to simulate in it.
Thanks,
Bhushan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bhushan,
You will need to download the PSpice model from the product folder and unzip it. Then from Orcad Capture click on File --> Open --> Design ... and then browse to the .DSN file in the unziped folder. When you open this, this should bring up the schematic along with the simulation profile. You can then run the simulation by simply clicking on PSpice --> Run.
Note that the trial version may have restrictions on the number of nodes in the circuit so if that is exceeded then you will not be able to run the simulation.
Best regards,
Bhushan,
There is a Manual.doc file and a What is included text file in the .zip file that will give you guidance for how to use the other files present.
Britt
Hi Nikhil,
Thanks you very much, sometimes while simulating the pspice models I face the more problems like convergence, divide by zero. Do you have any tips or docs please help. In tina-TI i dont know syntax for looking the current in branch.
Thanks and regards,
Bhushan
Hi Nagabhushana,
For TI's Power PSPICE & TINA-TI models, you can use the settings below. This should be a good starting point for most simulations and you can tune it from here for specific convergence errors. Divide by zero errors are a little more tricky. Generally they are a sign that the model may not have been constructed properly. However, sometimes I have seen that error disappear after I close PSpice and restart my machine so it might be a simulator issue as well.
|
PSpice Parameter |
TINA Parameter |
Starting Point |
When to change |
|
ITL1 |
DC max. iteration number |
1000-1500 |
For DC Bias Point and AC Convergence Issues |
|
ITL2 |
DC min. iteration number |
50 – 100 |
For DC Sweep Convergence Issues |
|
ITL4 |
TR max iteration number |
400 |
For Transient Convergence Issues |
|
RELTOL |
DC relative error |
1m |
For DC Bias Point, Transient and AC Convergence Issues |
|
VNTOL |
DC absolute voltage error |
10u |
For DC Bias Point, Transient and AC Convergence Issues |
|
ABSTOL |
DC absolute current error |
10n |
For DC Bias Point, Transient and AC Convergence Issues |
|
GMIN |
GMIN |
1p |
Try not to change this if possible |
|
Maximum Step Size |
TR maximum time step |
20n |
For Transient convergence issues, missing switching pulses, and similar issues. |
Best regards,