This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5009 using TINA TI

Other Parts Discussed in Thread: LM5009, TINA-TI

Hello everybody,

Using the excel sheet I got on the TI site, I've calculated the components for use with the LM5009. Then, with the transient model TINA TI Spice Model I got from TI site I tried to develop and simulate the circuit in TINA TI, but the results were very different from those expected. Someone can explain me what mistake I am doing?

Min Voltage 20 V

Max Voltage 95V

output 15V ( from excel datasheet )

Output Voltage from TINA TI simulations - less 1 V

Thks

 

LM5009_experiencia.TSC