Hi!
My SwitcherProDT not install in my computer.
Please see log .file
The following properties have been set:
Property: [AdminUser] = true {boolean}
Property: [ProcessorArchitecture] = Intel {string}
Property: [VersionNT] = 5.1.3 {version}
Running checks for package '.NET Framework 2.0 (x86)', phase BuildList
Running external check with command 'C:\DOCUME~1\TC23399\LOCALS~1\Temp\VSD2798.tmp\DotNetFX\dotnetchk.exe' and parameters ''
Process exited with code 1
Setting value '1 {int}' for property 'DotNetInstalled'
Reading value 'Version' of registry key 'HKLM\Software\Microsoft\Internet Explorer'
Read string value '6.0.2900.5512'
Setting value '6.0.2900.5512 {string}' for property 'IEVersion'
The following properties have been set for package '.NET Framework 2.0 (x86)':
Property: [DotNetInstalled] = 1 {int}
Property: [IEVersion] = 6.0.2900.5512 {string}
Running checks for command 'DotNetFX\instmsia.exe'
Result of running operator 'ValueExists' on property 'VersionNT': true
Result of checks for command 'DotNetFX\instmsia.exe' is 'Bypass'
Running checks for command 'DotNetFX\WindowsInstaller-KB893803-v2-x86.exe'
Result of running operator 'ValueExists' on property 'Version9x': false
Result of running operator 'VersionLessThan' on property 'VersionNT' and value '5.0.3': false
Result of running operator 'VersionGreaterThanOrEqualTo' on property 'VersionMsi' and value '3.0': true
Result of checks for command 'DotNetFX\WindowsInstaller-KB893803-v2-x86.exe' is 'Bypass'
Running checks for command 'DotNetFX\dotnetfx.exe'
Result of running operator 'ValueNotEqualTo' on property 'DotNetInstalled' and value '0': true
Result of checks for command 'DotNetFX\dotnetfx.exe' is 'Bypass'
'.NET Framework 2.0 (x86)' RunCheck result: No Install Needed
Running checks for package 'Windows Installer 3.1', phase BuildList
The following properties have been set for package 'Windows Installer 3.1':
Running checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe'
Result of running operator 'VersionGreaterThanOrEqualTo' on property 'VersionMsi' and value '3.1': true
Result of checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' is 'Bypass'
'Windows Installer 3.1' RunCheck result: No Install Needed
Running checks for package 'SQL Server Compact 3.5', phase BuildList
Reading value 'DesktopRuntimeVersion' of registry key 'HKLM\SOFTWARE\Microsoft\Microsoft SQL Server Compact Edition\v3.5\ENU'
Unable to read registry value
Not setting value for property 'ENU_INST'
Reading value 'System.Data.SqlServerCe.dll_ENU' of registry key 'HKLM\SOFTWARE\Microsoft\Microsoft SQL Server Compact Edition\v3.5\GAC'
Unable to read registry value
Not setting value for property 'ENU_INST_GAC'
The following properties have been set for package 'SQL Server Compact 3.5':
Running checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi'
Skipping ByPassIf because Property 'ENU_INST' was not defined
Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false
Result of checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi' is 'Install'
Running checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi'
Skipping ByPassIf because Property 'ENU_INST' was not defined
Result of running operator 'ValueExists' on property 'ENU_INST_GAC': false
Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false
Result of checks for command 'SQL Server Compact Edition\SSCERuntime-ENU.msi' is 'Install'
'SQL Server Compact 3.5' RunCheck result: Install Needed
EULA for components 'SQL Server Compact 3.5' was accepted.
Copying files to temporary directory "C:\DOCUME~1\TC23399\LOCALS~1\Temp\VSD2798.tmp\"
Downloading files to "C:\DOCUME~1\TC23399\LOCALS~1\Temp\VSD2798.tmp\"
(26/11/2009 14:31:50) Downloading 'SQL Server Compact Edition\SSCERuntime-ENU.msi' from 'http://go.microsoft.com/fwlink/?LinkId=115207&clcid=0x409' to 'C:\DOCUME~1\TC23399\LOCALS~1\Temp\VSD2798.tmp\'
Download completed at 26/11/2009 14:31:50
Downloading failed with HRESULT=-2146697211
Best regards.
Boris Sorokopud
RF & Communication Eng.
Elbit Systems Land and C4I - Tadiran Ltd.
P.O.Box 539
Haifa 31053
Israel.
Tel:(972)-4-8316018;
Fax:(972)-4-8316050.
E-mail:boris.sorokopud@elbitsystems.com
www.elbitsystems.com